This topic provides information on the closed loop settings located in the LTE Clause 8 test list under the Common Settings node. These settings configure how the instrument reacts to the input feedback signal configured in the instrument node and explained in the Closed Loop Feedback Configuration topic.
Makers provide an output signal to indicate when an event has occurred or to trigger an internal function. Each marker provides the same selections, but each marker can be set differently.
|
None |
No Marker signal. |
|
Frame Pulse |
Pulse at every 10 ms LTE radio frame |
|
Sub-Frame Pulse |
Pulse at every 1 ms LTE subframe |
|
Slot Pulse |
Pulse at every 0.5 ms slot |
|
Round Trip Time Pulse |
indicates the HARQ round trip time
|
|
HARQ State |
High for HARQ ACK received subframe Low for HARQ NACK received subframe |
|
ALC Control |
ALC signal to control RF output of the signal generator |
|
RF Blank |
RF Blank signal to control RF output of the signal generator |
|
Timing Adjustment Command |
Echo back of the received timing adjustment command (RS-232 serial data) |
|
Timing Adjustment State |
Indicates timing adjustment operation state |
|
SFN Pulse |
Pulse at every SFN 10.24s cycle |
|
AUX0...AUX15 Monitor |
Monitors the specified AUXn input signal. The timing of this output marker signal is not specified. This signal is available only to confirm that the AUX signal is being received on the expected port. |
The settings in this section tells the PXB or Signal Generator (instrument nodes) when to respond to the received feedback signal. The settings are the same for LTE FDD and TDD with the exception of the HARQ-ACK Input Sampling Position property. For LTE TDD, this property is inactive (grayed out).
For information on each setting, use the hints that appear when a property is clicked.